Applying InfoCenter Suite: Critical environments, energy and research organizations can reap the benefits
Critical Environments and the FDA’s 21 CFR Part 11
One of the most popular applications of InfoCenter Suite ® is to help companies regulated by the U.S. Food and Drug Administration (FDA) comply with the FDA’s rule for Electronic Records and Electronic Signatures (21 CFR Part 11).
The combination of InfoCenter Suite, Insight ® and the APOGEE ® building automation system provides the most technologically advanced solution to date for 21 CFR Part 11 compliance. This end-to-end solution provides complete management over the entire lifecycle of multiple types of records generated by the APOGEE Automation System.
While InfoCenter Suite 1.5 provides the long-term data management and reporting platform, the other components generate the relevant electronic records and protect their integrity until they are transferred to InfoCenter Suite. The new features of InfoCenter Suite 1.5—including Data Quality (see main article), New Security and Autogrow—— make InfoCenter a practical historian option for APOGEE’s compliance with FDA regulations.
For a pharmaceutical manufacturer, the complete compliance solution also requires validation and extended services. This validation often requires two distinct aspects. First, it is important to ensure that the software is working as designed. Secondly, it is important to ensure that software is applied correctly to support regulatory or compliance requirements.
Tracking energy usage to control costs
High energy prices have created a stronger need to understand where energy is being used and how to reduce consumption—especially in campus environments. One strategy is to sub-meter facility energy loads. Sub- metering provides valuable information in understanding energy usage and load profiles, but it results in large amounts of metering data.
InfoCenter Suite provides an excellent data storage and analysis platform for determining and understanding energy use patterns. It also assists in the complex task of managing the large volume of meter data. InfoCenter Suite 1.5—combined with options such as Utility Cost Manager, OPC client and APOGEE GO for InfoCenter Suite—can provide an effective option to produce centralized, web-based energy reporting. The result: Concise, readable reports that allow facilities managers to track energy usage and make critical decisions.
Colleges and universities: Ensuring top-quality R & D facilities
With state-of-the-art research and development facilities, a college or university can attract top-end students and faculty— and build collaborative programs with private industry. InfoCenter Suite provides fast, easy access to environmental system data to support and validate research studies. Scientists, doctors and technicians are able to focus on their research—not on the time-consuming tasks of retrieving and compiling supporting data.
For more information on the above three examples and more, send an e-mail message and it will be forwarded to your local Siemens Building Technologies office. Please include your full name, job title, name of organization, location and work telephone number.