|
New DEM
2000 measures energy consumption, demand and provides power diagnostic
information
Joining
the Digital Energy Monitor (DEM) 1000 is the DEM 2000. This family
of innovative, affordable meters -- from Siemens Building Technologies,
Inc., -- measure energy consumption (kWh) and demand (kW), and now
provides valuable power diagnostic information. A key component
of the Siemens solution for utility cost management, the DEM helps
managers improve the assessment, management and prediction of energy
costs. The new DEM 2000 now enables managers to not only better
understand their facility's energy usage but also gain insight on
the characteristics of the energy they are using. The digital power
transducers have direct connection to the Floor Level Network of
the APOGEE™ Automation System. And both series' transducers can
connect to new or existing field panels in the APOGEE system such
as the Modular Building Controller, Remote Building Controller,
Floor Level Network Controller or Stand-alone Control Unit.
The DEM family
combines a state-of-the-art communicating microprocessor-based power
transducer and high accuracy split-core instrument grade current
transformers in a single package. In addition to measuring energy
consumption and demand, the new DEM 2000 measures other power diagnostic
information such as apparent and reactive power, power factor and
a variety of voltage and current settings. Using the data, managers
can better understand energy baselines or load profiles, identify
equipment performance problems, determine equipment and system efficiency
solutions, forecast building demand, and support budgeting and cost
allocation applications.
"Traditionally,
customers use building automation systems to collect energy use
data, which requires separate meters to relay the signals back to
the field panel," says the Siemens Product Manager. "The DEM only
needs wiring for the direct connection to the Floor Level Network.
This unique design means fewer parts, reduced wiring and much lower
installation costs."
For more information
on the DEM 1000 or DEM
2000, contact your Siemens Building Technologies field
location.
APOGEE is a trademark of Siemens Building Technologies, Inc.
|